Part Number: TCA9555
Other Parts Discussed in Thread: TCA9539-Q1
Hello,
We use the TCA9555 chip to interface with a cable to turn on LEDs and be used as inputs for two buttons. P00 - P07, P10 power LEDs. P11 - P12 are inputs for two buttons. The port pins are driving the LEDs directly, we do not have them set up like in Fig 35 and Fig 36 of your datasheet. Unfortunately, we have the INT pin connected to a boot strap configuration pin that needs to be held high during initial boot. It looks like the INT pin holds the configuration pin low at random at initial boot. After measuring the pin at boot when the cable is connected to the TCA9555 chip and going through a power cycle, the INT pin acts crazy, as shown below:
When the cable is removed, the INT pin on the TCA9555 acts normal and allows the boot configuration pin to go high as intended:
What would be causing the INT pin to be acting crazy at boot? Is there a way to delay the interrupt pin from impacting the boot configuration? Are the ports driving the interrupt pin to go low at initial power on? Any insight would be greatly appreciated.