Part Number: DS80PCI810
We have made an adapter card from XMC to CPCI serial. When we remove the TI part and add wires, the card seems fully functional.
I have gone over the datasheet 3 or 4 times and can't find anything that we did wrong. I accidentally left the res3 pin open, but fixed that by shorting it to EQA pin right next door. GND through a 1K resistor.
The direction of the signals appears to be good. We are using pin strap mode with the values that are on the attached schematic. The chip is in 3.3V mode, and I verified there is 2.5 volts on all the VDD caps.
I'm really out of ideas, and we are about to just remove the part. Any help would be appreciated.
Thanks in advance.