This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: CSI-2 Data Lanes and Data Rates

Part Number: DS90UB960-Q1

Hi Team,

The 960 can do 1.6Gbps per data lane. If there are four data lanes, then a single CSI-2 port should be able to handle 6.4Gbps, correct? Since there are two CSI-2 ports on the 960, the total CSI-2 bandwidth can be 12.8Gbps, correct?

Thank you,

Jared