Part Number: DS92LV0422
Other Parts Discussed in Thread: DS92LV0421
Hi,
The customer uses DS92LV0421 / 0422 as a camera link product.
The camera link standard has a clock frequency of 20-85MHz,
which exceeds the SerDes clock frequency range,
but could be locked to 85MHz under customer conditions.
Therefore, They would like to estimate how much operating frequency margin the customer condition has.
How much are the temperature dependence and core voltage dependence of the operating frequency margin?
It does not have to be a guaranteed value.
[Customer conditions]
Temperature: -5 ~ 45 ℃
Deserializer core voltage: 1.8V
Best regards,
Yuto Sakai