Part Number: DS80PCI402
Hi Team,
My customer is evaluating DS80PCI402 with Electrical-to-Optical translation module, because communication between boards is optical fiber cable.
Since output differential signal from the E/O module increases gradually at start-up, and the system might cause PCI Express communication error at start-up.
If the DS80PCI402 had Squelch feature, it could not output signal while input signal level was lower than threshold level, they think.
The DS80PCI402 has Signal Detect feature, and the Signal Detect Threshold level is programmable.
Can the Signal Detect feature be used as the Squelch feature which they request?
Thank you.
Best Regards,
Koshi Ninomiya