Part Number: DS80PCI402
Hi Team,
My customer is evaluating the DS80PCI402 which is on the PCI Express add-in card. There are Electrical-to-Optical translation module and PCIe Switch IC on the board too. When they measured the case top temperature of DS80PCI402 under VDD=3.3V and Stand-by condition, it was around 80 degC at Ta=25 degC. Because the PCIe add-in card board itself became hot. And there are some communications even if it is stand-by condition.
Q1. Are there any difference of power dissipation between normal communication condition and stand-by condition?
Q2: Are there any difference of heat generation between normal communication condition and stand-by condition?
Please share your experience regarding power dissipation and heat generation of PCI express system.
Thank you.
Best Regards,
Koshi Ninomiya