This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867CR: About DP83867CR with 10 / 100BASE configuration

Part Number: DP83867CR

Hello.
This is a question when making a 10 / 100BASE only system with DP83867. If I make a 1000BASE system, I understand that four pairs of TD_P / N_A, TD_P / N_B, TD_P / N_C, and TD_P / N_D signals are connected to the connector via a transformer. In a 10 / 100BASE only system, two pairs of TX and RX signals are used. At that time, only TD_P / N_A and TD_P / N_B are used, and TD_P / N_A is connected as a TX pair via a transformer. , TD_P / N_B is connected to the connector as RX pair. (TD_P_A is 1pin, TD_N_A is 2pin, TD_P_B is 3pin, TD_N_B is 6pin) Will it be established with such a connection? I understand that it is reasonable to use a PHY device that supports only 10 / 100BASE. However, the client specifies that the PHY uses DP83867.

Regards.