Part Number: TCA6424A
Other Parts Discussed in Thread: TPD4E1U06
Hi
Because there is a problem at present, four white screens are displayed in the test (non-static test), three of which are always present, and the other is restored after a period of time;
The three machine are displayed white screens, which through log analysis, shows that the GPIO chip is abnormal, and one of the machines displays normal after replacing the new material;
Please help check if the schematic of TCA6424ARGJR is correct, PIN31 is 1.8V power supply, PIN27 is 5V power supply, and will reply as soon as possible.
The following is the relevant schematic:
GPIO Expend Interface part:

If our demand is the interface of GPIO Expend IC (TCA6424ARGJR) connection, the electrostatic voltage level that can be achieved is 15KV in air and 8KV in contact. The maximum electrostatic voltage of TCA6424ARGJR is 2KV, right? Is there a more suitable recommendation?
It's an urgent case.
Thanks a lot.
Best Regards
Elsa Duan