Hi team,
My customer used two pcs SN75LVDS83B in their two boards, named Board_A and Board_B.
In Board_A, SN75LVDS83B CLKSEL= VIH, which mean rising edge input clock trigger.
In Board_B, SN75LVDS83B CLKSEL= VIL, which mean falling edge input clock trigger.
They Used the same LCD screen with LVDS interface to connect respectively with Board_A and Board_B.
The result is that:
1. The LCD with Board_B, show the Font size is average in screen.
2. The LCD with Board_B, show the Font size is uneven in screen, some word's Font size is Thicker than other word.
Do you have any suggestions?
Thanks!