Part Number: DS90UH928Q-Q1
Hi Team,
My customer now is using DS90UH928 to pair DS90UB941.
How can they remove the HDCP to make compatibility to DS90UB941?
Only need to disable HDCP Debug1, HDCP Debug2 and HDCP status?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UH928Q-Q1
Hi Team,
My customer now is using DS90UH928 to pair DS90UB941.
How can they remove the HDCP to make compatibility to DS90UB941?
Only need to disable HDCP Debug1, HDCP Debug2 and HDCP status?
Amilie,
Yes, you are right, the difference just is to enable/disable HDCP function.
Rds,
Steven
you can check if the pattern has issue or not in both uh928 and ub941 side? it is always not a FPD-Link issue in this system.
btw, what is the test mode?
Regards,
Steven
Hi I can't understand how to check the pattern . Does the uh928 pin27(lock) & pin28(pass) high means ok?
or just what I said test mode which from document snla132d.pdf (Exploring the Int Test Pattern Generation Feature of FPD-Link III IVI Devices).
Thank you
Yes, please follow up the pattern gen. app. note to run the pattern with internal clock in the uh928 and ub941as respectively, and observer how the panel displays? if the uh928 internal pattern with internal clock timing and PCLK can make the panel display well?
best regards,
Steven