Part Number: DS90UB953-Q1
hello,team
I have 2 questions about SNLA270A,UB953 work with UB914
one is that there is a note that YUV 8bit format is not supported
can we use YUV422 10bit mode to transmit YUV422 8bit data while upper 2bits have no data
or can we use YUV422 12bit-HF mode to transmit YUV422 8bit while upper 4bits have no data
another one is how to calculate total Parallel output that is going to be sent out from the 914 and into Processor
if output format is YUV422 10bit+HS+VS+CLK ( clk=96MHZ) active pixel 1280*800@30 fps ,total timing with blanking is 1905*840@30fps
total Parallel output is 96MHZ*10bit=960Mbps ,right or wrong?