Part Number: TRS232E
Other Parts Discussed in Thread: MAX202, TRS202E
Hi Sir
May TRS232EIPW can direct to replace MAX202CUE?
what is TRS232EIPW benefit to replace MAX202CUE?
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bogey,
I would recommend TRS202E to be able to use 0.1uF charge pump capacitors which are specified in MAX202 datasheet. TRS232E suggests using 1.0 uF capacitors. TRS202EIPW will offer an operating temperature range from -30 to 85 C and ESD protection on RS232 pins. In comparison, MAX202CUE+ shows an operating temp range of 0 to 70 C and MAX202 datasheet does not specify ESD protection.
Let me know if you have any more questions.
Regards,
Eric