This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: Image data latency

Part Number: DS90UB953-Q1


Hi,

I received a response from Casey about the latency from csi input of 953 to CSI output of 960 to be upto 2 lines. an additional question about this is if this 2 lines is fixed for any given length of POC cable (2m, 10m, 15m)? Or will there be any delay computation factoring the POC cable length and FC clock speed?

I'm also wondering possible effects of ambient temperature to signal latency. Are there any application notes i can refer to?

Thanks for the response!

Regards,

Laud...