This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: FPDLink Deserializer to CSI2 That Supports 5Gbps per lane

Part Number: DS90UB960-Q1

Interface Experts,

Greetings!  I received a question on another forum where Alex (customer) wants to know if we have any options to support deserializer input FPD-Link-III line rate over 5 Gpbs.  The output should support CSI2.  

I am asking Alex which serializer (brand, model#) he plans to use.  In the interim, I searched on TI and looks like our highest deserializer FPD-Link-III line rate is rated for 4.16 Gbps (UB960).  However, since this is outside my expertise I am re-posting the question here.  Can you help recommend another module Alex may be able to use?

I will re-route Alex to this forum so he can converse with you directly.

Thank you!

Best,

Shiou Mei