Part Number: DS90UB934-Q1
Other Parts Discussed in Thread: DS90UB935-Q1
I am using a CSI-2 image sensor, DS90UB935-Q1 serializer, DS90UB934-Q1 deserializer, and DVP input image processor. The data is RAW10 with DVP backwards compatible mode.
I will include a timing diagram showing the active video as well as inactive and blanking periods.
According to the previous related thread: The DVP HSYNC signal is generated based on "LP transitions" of CSI-2 input, which are part of the SOT/EOT in the CSI-2 timing diagram. The DVP VSYNC signal is generated according to FS/FE. The timing diagram is drawn on this basis.
What happens in periods B, C, G, H which are outside the active video but inside the HSYNC high time? Are the PH/PF (packet header / packet footer) passed through to the deserializer output?
During blanking, will the data output have a fixed value (for example, all zeros) ? Which periods on the timing diagram will be affected?
Also, can you confirm the HSYNC will stop running during frame blanking?
Your assistance is appreciated!
--
Daniel Doonan