This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Power consumption under Standby Mode

Part Number: DP83867IR

Hi Team,

My customer is evaluating DP83867IR. When they measured input current of +2.5V for VDDIO and VDDA2P5 under Normal Operation and Standby Mode, input current under Standby Mode was higher than that under Normal Operation. During Normal Operation, LinkUp is established.
  - Standby Mode: Set Bit-2="1b" of "PHY Control Register (PHYCR), Address 0x0010"
  - VDDIO=2.5V
  - VDDA2P5=2.5V
  - VDDA1P8=unused
Do you think that is correct power consumption of the DP83867IR?
Thank you.

Best Regards,

Koshi Ninomiya