Part Number: DP83822EVM
Other Parts Discussed in Thread: USB-2-MDIO,
Hi team,
There are my testing step.
1. I used USB-2-MDIO to set DP83822EVM Analog loopback mode following below Register setting;
2. I sent the data=0xa5 to DP83822EVM by MII and enbale TX_EN.
But I can't catch any waveform from RX_D[0:3] pin, which mean there are not any loopback data.
I saw the user guide that it need 100 Ω termination in TX/ RX pins.
But I saw the DP83822EVM SCH and there are two 49.9Ω pull-up in TX/ RX pins. So in my mind, it don't need 100 Ω termination in TX/ RX pins, right?
If yes, why can't I catch any waveform from RX_D[0:3] pin?
Thanks!
Register setting:
begin 001F 8000 //software reset (clears register)
0000 2100 //programs DUT to 100BASE-TX mode
0019 0021 //programs DUT to Forced MDI mode, set to 4021 for MDIX mode
0016 0108 //enables analog loopback mode
001F 4000 //digital reset (doesn’t clear register)
end