Part Number: DS160PR410
Hi,
Does DS160PR410 supports DC coupling interface or AC coupling only?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS160PR410
Hi,
Does DS160PR410 supports DC coupling interface or AC coupling only?
Thanks,
Hello-
The DS160PR410 high-speed I/Os need to be ac-coupled.
Regards,
Davor
Hi,
- What is the internal DS160PR410 Rx terminations and what is the voltage it is terminated to?
- What is the internal DS160PR410 Tx terminations and what is the voltage it is terminated to?
- can I set a DC coupling between my transmitter to DS160PR410 Rx while remaining same offset DC as DS160PR410 Rx side?
- can I set a DC coupling between my reciever to DS160PR410 Tx while remaining same offset DC as DS160PR410 Tx side?
Thanks,
Hello-
On the RX side, there are 50-ohm terminations to 2.5V bias via an active switch. DC coupling the DS160PR410 RX pins may reduce reliability of the termination resistors as these can handle very limited current.
On the TX side, there are 50-ohm terminations to 0.75V. DC coupling the DS160PR410 TX pins poses a risk to the reliability of the termination resistors as these can handle very limited current.
The DS160PR410 high-speed I/Os need to be ac-coupled. DC-coupling is not recommended.
Regards,
Davor
Hi,
The input common mode voltage on the DS160PR410 RX is affected by an active switch. The delta between 2.5V on your TX side and the input common mode voltage on the DS160PR410 RX could still be significant enough to cause reliability issues with the input termination resistors.
The DS160PR410 high-speed I/Os need to be ac-coupled. DC-coupling is not recommended.
Regards,
Davor