Hi Team,
May I ask if 949 's INTB connect to 1.8V(VDDIO-949) but 948's INTB connect to 3.3V(VDDIO-948), is it ok?
Do we need to keep 949 and 948 INTB connect to the same voltage level (both 1.8V or 3.3V)?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
May I ask if 949 's INTB connect to 1.8V(VDDIO-949) but 948's INTB connect to 3.3V(VDDIO-948), is it ok?
Do we need to keep 949 and 948 INTB connect to the same voltage level (both 1.8V or 3.3V)?
Thanks!
Hello Amelie,
The voltages do not need to match on the serializer and deserializer sides.
Best Regards,
Casey