Part Number: TCA9803
Hello guys,
One of my customers is evaluating TCA9803 for their new products.
In the evaluation, they connected the master device to side A of TCA9803 and a slave device to side B.
Also VCCA and VCCB are 3.3V.
Then they faced I2C communication error after about 100us clock stretching only.
They found the cause. The cause was SDA_B voltage falling speed is slower than regular acknowleage action.
The phenomenon is happened only after the clock stretching.
I know TCA9803 has internal constant current circuit for side B pulling up.
Is the internal constant current changed between regular acknowledge action and after 100us clock stretching action?
Your reply would be much appreciated.
Best regards,
Kazuya.