This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Using two cameras with different resolutions and frame rates, replication?

Part Number: DS90UB954-Q1


Hi Team,

I have a 2 camera application that uses the DS90UB954-Q1, its a 1.7M and 1M cameras that will work simultaneously and will need to replicate and forward this data  like shown in figure 53 of the datasheet. I want to verify my thoughts to see if this is a possible applications. 

The BW requirements from the cameras will be the following. From the bandwidth perspective it looks possible to aggregate the camera inputs on 2 lanes and use the other  2 lanes to replicate each camera input. Is this correct?

12bits x 1.7M x 36FPS  x 1.3Overhead =~ 954 Mbps

10bitx 1M x 36 FPS x 1.3 Overhead =~468Mbps

I saw the following post and i beleive it confirms my thoughts above but want to verify i am not missing anything.

https://e2e.ti.com/support/interface/f/138/t/805084