Part Number: SN65HVD1050-EP
Other Parts Discussed in Thread: SN65HVDA1050A-Q1, SN65HVD1050-Q1
Hi Team,
Related to the question in the other thread:
In the datasheet, it is stated that it withstands voltage transients from –200 V to 200 V, according to ISO 7637. However, the training that was linked to in the previous thread only provides information about the ISO7637 standard. Since the +/-200V is not part of the regular ISO7637 tests, there is no information about it in the standard.
Could you please share details about the transients used for the testing of the device?
Regards
Mihir