Part Number: HD3SS3411
Hi,
Is that part can be recommended for 2:1 clock mux LVDS input and HCSL output drived for a pcie gen3 application?
Regards,
JL
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HD3SS3411
Hi,
Is that part can be recommended for 2:1 clock mux LVDS input and HCSL output drived for a pcie gen3 application?
Regards,
JL
Hi JL,
I do not see a reason what it could not be used for this type of application. The PCIe electrical characteristics match with the HD3SS3411 switch.
The differential crosstalk is quite low at -35dB @ 4 GHz, I would expect it to improve further when dealing with lower frequencies associated with a 100 MHz PCIe clock signal.
Regards,
Lee