Part Number: AM26C32
Hi Team,
I would like to confirm about below basic things related to Table 1, could you answer those?
(1) May I think VID definition as below?
VID = “Input voltage on A” – “Input voltage on B”
(2) DIFFERENTIAL INPUT in Table 1, VID >= VIT+
VIT+ is defined as 200mV as max (with VIC=-7V to 7V).
IF G=H, and VID (in above definition) > 200mV, will OUTPUT be H?
(3) DIFFERENTIAL INPUT in Table 1, VIT < VID < VID+
Regardless G or nG setting, if VID is between VIT- and VID+, will the OUTPUT undefined?
Best regards,