This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I would like to confirm about below basic things related to Table 1, could you answer those?
(1) May I think VID definition as below?
VID = “Input voltage on A” – “Input voltage on B”
(2) DIFFERENTIAL INPUT in Table 1, VID >= VIT+
VIT+ is defined as 200mV as max (with VIC=-7V to 7V).
IF G=H, and VID (in above definition) > 200mV, will OUTPUT be H?
(3) DIFFERENTIAL INPUT in Table 1, VIT < VID < VID+
Regardless G or nG setting, if VID is between VIT- and VID+, will the OUTPUT undefined?
Best regards,
Hi Nobuo-san,
(1) VID = “Input voltage on A” – “Input voltage on B”
Yes, this is the correct definition: VID = VA - VB
(2) IF G=H, and VID (in above definition) > 200mV, will OUTPUT be H?
Yes. When the device is enabled (G=H or nG=L) and the input differential is above the defined threshold (VID ≥ VTH+), the output will be high (Y=H).
(3) Regardless G or nG setting, if VID is between VIT- and VID+, will the OUTPUT undefined?
When the device is enabled (G=H or nG=L) and the input differential is between defined thresholds (VTH- ≤ VID ≤ VTH+), the output is undefined (Y=?). If the device is disabled (G=L and nG=H) and the same conditions appear on the input differential (VTH- ≤ VID ≤ VTH+), the output will be high-z (Y=Z). This is because in this enable state (G=L and nG=H) the input differential is a don't-care (x).
I hope this helps. Let me know if you have any more questions.
Regards,
Eric