Part Number: TVP7002
Hi All,
I have a requirement to drive a display which can be interfaced using HDMI cable. The contents of the display will be generated dynamically in C code. I have earlier considered Beagle Bone Black to do the job, but my requirement is as follows:
1. The system should not use LINUX OS, preferably a non OS based system is intended
2. The system must boot as fast as possible (no several seconds time taken for boot like LINUX OS)
Can anyone suggest me a TI MCU which can be readily interfaced to chips like TVP7002 or NXP19988 (as used in BBB) to generate the HDMI signal? I am looking for an MCU which will give the 3x 8 bit data for the video along with the sync signals. Am also looking for supporting example codes for the MCU.
Regards
Soumyajit Das