Part Number: TUSB8041
Hi Sir,
I have a design of hub USB 3.0 with the TUSB8041I.
The host controller (upstream side) is directly provided by the CPU, downstream is 4 port USB3.0 Type-A connector.
The CPU side is replaceable. When the CPU uses the Intel Broadwell-DE platform, USB 3.0 functions normally. When using Intel Skylake-D CPU, it cannot recognize USB3.0 devices but can recognize USB2.0 devices.
I have tested that the upstream USB 3.0 signal can normally identify the USB 3.0 device, while the downstream the eye diagram measurement result is a pass.
Would you do me a favor?