This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Serializer/deserializer HDMI (TMDS) to MIPI CSI-2 for 4K camera



Hey!

I have looked through the available products and cannot find a solution to my problem. I require to connect 4K camera ie: Sony FCB-ER8300 or Sony FCB-ER8230 to NVIDIA Jetson TX2 w/ a development kit. There exists a pair of SerDes for LVDS to MIPI CSI-2 for a camera like Sony FCB-EV7520A, but these cameras have much higher frequency 296.703 MHz.

I need a pair of serializer and deserializer to convert from HDMI (TMDS) to a single wire and then single wire to MIPI CSI-2, that's the want ... but all possibilities are acceptable.

Thanks in advance!