Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65988
We have a new problem with configuration of the PD-controller TPS65987D.
After the short circuit test below we have changed the configuration of the TPS65987D. This has caused erroneous behavior, verified on several boards. Initially, after configuration, the behavior is correct. When connecting a device first time it is ok. After that when disconnecting the USB-cable the VBUS voltage remains +5V despite the configuration status is ‘No plug present’! See the attached document. (The same board works well with another configuration of the TPS65987D.)
The complete configuration downloaded from the CPU is defined in the second document. (The flash IC34 is empty.)
Is this a configuration that should be ok?