Hi TI,
I'm working on an Alpine Ridge two port self powered Thunderbolt design that supports 5V @ 3A out from both ports. I have the TPS65983 tool version 6.12
Should I use the project "Apex Creek ATX" for this?
Do I make any changes to the configuration of the TPS65983 in the customization tool after I've opened the Apex Creek ATX project? Do I just save the bin file and use it with all the defaults?
Under transmit source capabilities, there are 4 "Source PDO" profiles from 5V @ 3A up to 20V @ 3A. My product can only support the "Source PDO 1" Do I leave the other Source PDO profiles as they are?
For Thunderbolt certification I need to submit a form called: “PD VIF Excel format required” I don't know what that is, can you point me to something which explains this?
Thank You,
Rob Sherman