Part Number: PCA9306
I am considering using the PCA9306DQER in a design where the master side is 3.3V and the slave side is 1.8V. The datasheet indicates that the lower voltage is connected to Vref1 and also that this is the master side. In my intended use the master side will be the higher voltage. Will there be any problems if I connect the Master side of 3.3V to vref2 and the slave side of 1.8V to vref1?