Part Number: DS90UB936-Q1
Hi TI,
Could you pls help me comprehend FPD3_CLK? when will use this clk?
BR
jason_koo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB936-Q1
Hi TI,
Could you pls help me comprehend FPD3_CLK? when will use this clk?
BR
jason_koo
Hello Jason,
For CSI-2 modes the FPD3_PCLK is the frequency of the FPD-Link forward channel frames. The frame size is 40 bits so with FPD3_PCLK = 100MHz, the forward channel rate is 4Gbps. You can use this calculation to determine rates of the device and the input jitter tolerance in table 5.
Best Regards,
Casey
hi casey,
Got it, FPD3_PCLK is the data package clk of fpdlink line.
Tks
jason