Part Number: SN75LVDS83B
Hi,
We are using SN75LVDS83B to convert RGB (18 bits CPU) to a 10.1 display LVDS (24 bits) display.
We facing problems with the image. The colors is not good and there is a lot of noises either.
The image below is the linux boot sequence. Note there is a noise on Tux image.
The next is the linux desktop. It should be like this - docs.toradex.com/101143-image-toradexlinuxdesktop.jpg

Next image is the schematic and connections.
Note we connect the Y3 signal, but nothing changes.
Any one here already have this problem?
We appreciate any help!
Thanks!