Part Number: DP83825I
Other Parts Discussed in Thread: DP83825EVM
My customer has struggled due to compliance test of Voltage level failure as attached one.
Please advise how to fix it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83825I
Other Parts Discussed in Thread: DP83825EVM
My customer has struggled due to compliance test of Voltage level failure as attached one.
Please advise how to fix it?
Please also share TI's evaluation results as well. Thanks.
Hi Hironori,
Here is the app note to our compliance testing instructions and results.
http://www.ti.com/lit/an/snla239a/snla239a.pdf
http://www.ti.com/lit/an/snla266/snla266.pdf
Best,
Cecilia
Cecilia, You have attached wrong PID. I am asking on DP83825I.
Hironori Yoshimura
Please check attached file. This is similar results on the TI's ref EVM.
Please kindly advise how to fix ?
Hi Hironori,
Do you have a schematic of the design? You are not using the DP83825EVM, correct?
Thanks,
Cecilia
Two files are. one is customer's own design and next result is on the TI DP83825I EVM results.
We are facing same results. probably we have to adjust something Register setting ?
Hi Hironori
Yes that could be one possibility. Can you please share the register settings for both boards? Also can you confirm you are using the correct RBIAS value at 1% tolerance?
Thanks,
Cecilia
> 100 Base Standard MDI (Test Mode 5)
> Reg 0x001F = 0x8000 //reset PHY
> Reg 0x0000 = 0x2100 //programs DUT to 100Base-TX Mode
> Reg 0x0010 = 0x5008 //programs DUT to Forced MDI Mode
> Reg 0x0009 = 0xBB00 //Test Mode 5
> Reg 0x0025 = 0x0480 //output test mode to all channels
RBIAS is 1%.
Can you read all values? I would like to review all registers and in particularly register 0x0403.
Thanks,
Cecilia
Customer only control Test register as mentioned above. That all.
I could not find 0x0403 from datasheet register map. What is looking for ?
Please specify specfic register what you want to see. My customer just applied TI's EVM and it is failing as attached waveform.
Any suggestions , please advise me.
I see that you have only written into those registers that you mentioned above, however, are you able to read all registers? Register 0x0403 should help with the line driver voltage swing which would help your compliance failure.
Thanks,
Cecilia