Part Number: DS160PR410
Data sheet specifies the resistors to be used for the L0-L3 levels as being 1K, 13K and 59K
In the eval board user guide SNLU252A figure 11, the resistors used for setting the I2C adders match the values above.
However, the resistors used for setting the levels for VOD_DS are 249, 3.24K and 14.7K
Same figure 11, the resistors for setting GAIN and RXDET are 14.7K
Could explain which values I should use?