This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: Three-Supply Mode - Wait before ramping 1P0

Part Number: DP83867IS

A customer is asking regarding the DPS83867IS.

- Assuming the 2.5V and 1.8V rails are ramped first, is there any maximum time limit before needing the 1.0V rail powered up?

- In other words, if 2.5V and 1.8V are powered and the 1.0V rail is not, will the device experience any kind of breakdown or lifetime degradation?

I don't believe there are any diodes between the 1.0V rail and the others, so I am assuming reverse current isn't a problem...anything else that could happen?

ramping