Part Number: P82B715
Other Parts Discussed in Thread: P82B96
Hi,
I'm trying to read the inclination angle from my inclinometer, my main board(MCU) is connected to accelerometer (located on daughter board) via a 1 meter (4 core shielded) cable, as shown in below attached document. The schematics of the connectivity of MCU, I2C buffer, RTC IC (excluding cable & Inclinometer) are present in the last page of the attached word document, please refer.
U17---> I2C buffer (P82B715)
U10--->RTC IC (DS3232SN#)
When I tried to read the inclination angle, I'm getting as "Inclinometer Error" on putty as shown in attached image for not working board. But with the same cable I'm able to read correct data using another working board, there I'm able to see the (X-axis) angles, please go through the images attached. So I guess there is no issues with the cable & daughter card. I've checked continuity & parts around the U10, U17 ICs they are fine.
I2C buffer & RTC IC are sharing the common I2C bus from MCU. I've measured the voltages at SDA, SCL pins of U10 IC, then I got 2.1V around. Then I tried to measure SDA, SCL pin voltages at RTC IC, by removing U17(P82B715) IC, then I got around 3.1V on them. So then I replaced with new P82B715 IC , but now I got 2.1V. I am getting "??" symbols while tried to input time to RTC IC due to this I guess.
All the other working boards are pulled to 3.3V only, i'm able to get valid X-axis values on putty.
I have measured the voltages on U17 IC at SDA, SCL, LX, LY pins of working & not working boards using Oscilloscope, please find them in attachments, similarly for U10 IC measured SDA, SCL both working & not working boards.
Please suggest me how to proceed.
All the required images are placed in the attached MS Document file, please go thorugh.
Thank you in advance.