Part Number: DP83822I
Other Parts Discussed in Thread: DP83822EVM
Hello, thanks again for your support.
after an in depth analysis of the Ethernet phys layout we realized that there are layout problems with our prototype.
The prototype is part of a bigger system which will be realized with two layered boards. The MCU, implementing the MAC, is paced in the top layer. It is connected via flat cables to the lower layer which, amongst all, hosts the eth connector and magnetics. In this first prototype the physical was placed in the upper layer, so the diff signal was sent down to the magnetics via connector and a short flat cable. An additional 5-6cm path is then followed by the signal prior to get to the magnetics and finally to the connector.
I am firmly convinced that this contradicts your guidelines and I think the optimal solution would be sending to the lower layer the RMII signals (unbalanced and at a lower frequency) putting the phys (dp83822i) as close as possible to magnetics.
I need your feedback on the matter along with your detailed guidelines for the phys layout (with what must and must not) be done.
thanks again in advance for your valuable support.
Best regards,
GZ