Hi All,
I have a new design using three DP83867CS PHYs and NXP T2081 MAC. I have the PHY addresses as 0, 1 & 2. The previous design used different PHYs but we changed them out to add additional functionality. The previous design PHY addresses were 1, 2 & 3. When we plug Ethernet cables in the PHYs appear to link up just fine. The problem is with the MDIO signal. It's very low, may .5V. It's pulled up with a 1.5K resistor. I double checked the schematic symbol, all pins numbers are correct, power etc. I've done dozens of Ethernet designs and have not seen this before. I was able to cut the PCB trace on MDIO on the last PHY and the signal level went up to about .9V. Both of our prototypes are doing the same thing.
My first question is, is PHY address 0 valid? I seem to read conflicting information on this. Any, any ideas? Has anyone seen this before?
Thanks!