This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84: Will this part support 2 independent LVDS display at a time?

Part Number: SN65DSI84

Hi,

I would like to get a clarification on this part to support 2 LVDS display. My MIPI input to this Bridge is of 1080p resolution ,Can SN65DSI84 part support 

1) Two independent LVDS displays with each 1080p resolution at the same time ? or 

if yes-Can it support two  LVDS panels with video content different or same on both LVDS displays ?

How is the Clock configuration can be taken if 2 Display support is there.

Please help us on this what are the constraints if i want to use 2 LVDS panels. 

Regards,

Shruthi