Part Number: DS90UB954-Q1
Hi team,
We have questions about UB954 and UB933 cooperation for encoding and decoding.
DS90UB933: Input format:YUV422-8Bit
Operating mode:10-bit Mode,but only use DIN[7:0]
In this configuration of UB933, we configure the UB954 register 0x70 = 0x1E(Only one input),register 0x7C = 0xC1.
Can this configuration decode the signal transmitted from 933 correctly.Now that our configuration has abnormal colors on the display side, we suspect that U or V signal is missing two of them
Best regards,
Alec Li