Part Number: DS15BR400
Dear TI associate, back in January of 2020 Lee replied back to Lindsey as:
Hi Lindsey,
The unused inputs should be tied off as listed below to ensure the outputs remain in a stable state.
IN+ = 3.3K to VDD
IN- = 3.3K to GND
This will ensure 50mV of offset at the input which is enough to keep the output from switching.
Regards,
Lee
We have the same issue, with no cable attached while providing 68mV of DC bias delta between the plus and minus inputs of the part, we are still observing 100mV of oscillation at the out plus pin. Is there a way to get rid of this oscillation? The output is not switching between high and low level which is a good thing, however the plus side oscilating is not of favor.
The part's case temperature is around 70C, when idle, is this normal? We followed the layout guidelines by providing 5 x 0.2mm size vias to GND plane on middle thermal pad. I look forward to your response.
Thanks,
Bahram