Other Parts Discussed in Thread: DP83869
Hi, I'm using DP83869 as a 1000M media convertor for . I'm not sure for the following questions.
1. .Is SD(Pin no. 24) pin a high valid or a low valid input? The datasheet did not specify the polarity or functionality of the SD pin. The LOS pin is a low value when the signal is good for SFP modules but SD pin is high for a SFF module. And then, should I connect DP83869's SD pin to SFP's LOS directly and with an inverter to SFF's SD, or in an opposite way?
2. Do I need to place 100-Ω termination resistor between the differential pair lines link SGMII and Magnetics copper PHY? It did not say if the termination resister is needed or not. There's no terminal resister in EVM schematic.
3.I only want to have the media convertor with resistor straps and don't want to use any MCU. Can be DP68389 used as a media convertor only with strap pins configuration? It's not very clear in datasheet and the saying is opposite in this form. John confirms that it work well with just strapping pins but Aniruddha said software access is needed to work in media convertor mode.
https://e2e.ti.com/support/interface/f/138/t/769396?tisearch=e2e-sitesearch&keymatch=DP83869
| 100-Ω termination |