Part Number: SN65HVD08
Hi,
I am trying to use the part SN65HVD08 connecting to a Modbus slave on one side and the other to the USB-UART cable https://www.digikey.ca/en/products/detail/ftdi-future-technology-devices-international-ltd/TTL-234X-5V/6823719.
Here I have implemented the Application circuit mentioned at the Page 19 of the datasheet of SN65HVD08 except the Direction control line connection .
I am using Modbus Scan simulator tool and I am not seeing any response here and it looks like everything else is correct. I sense here if the Direction line has to be controlled high and low.
I tried with pulling down the /RE and pulling up the DE at the same time to permanently enable the direction flow in both directions but looks like it does not work either. Does it has to do with the RTS and DTR setting of the connection setup in Modbus simulator tool ?
(The setup otherwise works good with MAX1387 based circuit where there is no direction control required)
Thanks
Abhishek