Part Number: PCA9518
Other Parts Discussed in Thread: PCA9306, TCA9517
Hi team,
From P6 of the data sheet, it means that VIH=0.7*Vcc-5.5V. If Vcc=3.3V, VIH=2.31-5.5V so it seems that there is no problem using 2.8V.
However there is the following description in P3 of the data sheet,
“The device is designed for 3-V to 3.6-V VCC operation, but it has 5-V tolerant I2C and enable (EN) input pins.
This feature allows for translation from 3 V to 5 V between a master and slave.”
I2C(SDAx/SCLx) and EN pin can operate at 3-5V, that is, 2.8V pull-up cannot be used. Is it correct?
If we are trying to connect an IC that requires 2.8V pull-up and if PCA9518 does not support 2.8V pull-up, we need to prepare a level shifter, so I've confirmed it just in case.
Beat Regards,
Tom Liu