Part Number: DP83867IR
Hi,
My customer would like to know below connection between DP83867 and RJ45 terminal.
| DP83867 PIN | RJ45 |
|
TD_P_A |
6 |
|
TD_M_A |
3 |
|
TD_P_B |
2 |
|
TD_M_B |
1 |
|
TD_P_C |
8 |
|
TD_M_C |
7 |
|
TD_P_D |
5 |
|
TD_P_D |
4 |
Is it possible to connect above connection?
The connection between EtherPHY and RJ45 Usually connect as below,:
However, DP83867 EVM connection are below:
In EVM, the order of PIN number of RJ45 is opposite from normal connection. For example, PIN 1 of RJ45 connects to TD_D_N but the PIN1 connect to TD_P_A. It looks like DP83867 can automatically detect and connect for both case, then, customer would like to know if the device can automatically detect and connect his own connection.
Regards,
Nagata.