Hi Team,
I am just confused why there are two groups of I2C in 964? In what situation customer will use two group?
If I only use one group, just need to left the second group I2C float?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I am just confused why there are two groups of I2C in 964? In what situation customer will use two group?
If I only use one group, just need to left the second group I2C float?
Hello Amelie,
The two I2C ports allow multiple processors or MCUs to communicate with 964 simultaneously. For example, in a system design where two processors receive CSI-2 input from 964 (which has two CSI-2 output ports), each processor can independently communicate with the FPD-Link hub. Using the second I2C port is completely optional. It is recommended to tie both I2C ports up with the datasheet recommended pullups to VDDIO to prevent false toggling - do not leave these pins floating
Best Regards,
Casey