Part Number: DS64BR111
Other Parts Discussed in Thread: DS100BR111, DS100BR210
Hi Team,
I am looking for a driver/buffer IC that can drive the input of SFP(4.25Gbps) transceiver.
・FPGA outputs CML signal on the board and inputs it to SFP.
・The specifications of SFP is attached.
80-21-0541 A5WLSN85ADMA0541 001 (2).pdf
In this design, we think that the distance from the FPGA to the SFP module is about 3 cm and the loss of PWB is not so large, rather, we think that the signal jitter due to the insertion of the driver device is the problem.
So I would like to confirm the basics with the following devices.
DS64BR111
DS100BR111
DS100BR210
・Can I use the default setting after power-on without using SMBus serial programming?
・Can I use frequencies below 10Gbps, such as 4.25Gbps?
・Which of the above devices has good jitter performance?
Beat Regards,
Tom Liu