Part Number: TCA9800
Other Parts Discussed in Thread: TCA9511A
Hi expert
Could you please let me know your recommended I2C buffer device for the following condition?
We proposed TCA9800/1/2/3. however, input resistance spec <150ohm.
The drive current in the Host device is weak. IOL=0.63mA, VOL=0.36V, 571ohm.
The drive current in the slave device is also weak. IOL=1.0mA, VOL=0.36V, 360ohm.
Thanks
Muk