Part Number: SN65HVDA1050A-Q1
Other Parts Discussed in Thread: SN65HVD251, TCAN1051
Hello,
I'm redesigning my automotive scan tool and I want to use the SN65HVD251 instead of SN65HVDA1050AQDRQ1. The only relevant difference I found between them was the hysteresis of the receiver which for the model SN65HVDA1050AQDRQ1 is 125mV while for the model SN65HVD251 it is 100mV. The two ICs are very similar, but the SN65HVDA1050AQDRQ1 is cheaper.
I know that SN65HVD251 can work with Single Wire CAN, but I don't know the same about SN65HVDA1050AQDRQ1 .
So, What would be the impact of using the SN65HVDA1050AQDRQ1 instead of SN65HVD251 ?
Regards,
Daniel.